Cancel
Showing results for 
Search instead for 
Did you mean: 

process simulate with conveyor tracking

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

hi,

 

is it possible to move a part on conveyor 1 pick on end with robot and drop to next conveyor?

 

i found no way to attach the moving part after handling (from rob) to secound conveyor.

 

first conveyor works fine

secound conveyor ???

 

thanks

Kind regards,

Benjamin Voelzke
4 REPLIES

Re: process simulate with conveyor tracking

Siemens Phenom Siemens Phenom
Siemens Phenom

This should work, I would say the two following things must be fullfilled:

- Appearance defined as "Conveyable Part".

- The Conveying Frame should have contact to the "Conveying Surface".

 

I did something similar but without robot handling:

Conv1 --------> Conv2

Then the part is at the end of Conv1 its automatically handover to Conv2.

 

Re: process simulate with conveyor tracking

Pioneer
Pioneer
hi,
this is flow operation in operation tab of ps, but we don't know it's the right one that you need whether or not.
paul

Re: process simulate with conveyor tracking

Siemens Phenom Siemens Phenom
Siemens Phenom

There is no flow operation in use.

 

Using conveyor simulation requires LineSimulation Mode.

Move part along a conveyor ----> Pick Part with robot ----> Place Part on other Conveyor ---> Move part along second conveyor.

 

In my video, it´s also LineSimulation Mode two conveyors where the part is moved along conv1 and after it reaches the end it´s handover to conv2.

 

Best regards

Patrick

 

 

Re: process simulate with conveyor tracking

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

thanks for info.

 

it's works correct with 2 conveyors.

 

Kind regards,

Benjamin Voelzke