Cancel
Showing results for 
Search instead for 
Did you mean: 

ps 13.1.1 with plcsim adv. connection

Gears Phenom Gears Phenom
Gears Phenom

hi,

 

is it possible to connect the plcsim adv. and read only a signal from other psa partner?

 

ex.

tool 1 is connected to psa and write gripper signals

 

tool 2 is connected to same psa connection and write signals for safety

 

tool 3 (PS) is connected to same psa

my wish:

i will read and present the status from other signals (gripper or safety) in ps

 

is it possible?

 

thanks

Kind regards,

Benjamin Voelzke
1 REPLY

Re: ps 13.1.1 with plcsim adv. connection

Siemens Legend Siemens Legend
Siemens Legend

Hi

 

No. This is not possible today.

 

PS reads only Input signals from the PLCSIM Advanced instance and writes Outputs to it so triggering an Input signal from another source will not be evident in Process Simulate.

 

 

 

 

Kind regards,
Gal Snir