Cancel
Showing results for 
Search instead for 
Did you mean: 

question about process simulate logic in simulation layer ( DECL CHAR ATEC-VAR[10] )

Gears Phenom Gears Phenom
Gears Phenom

my problem nr 1:

i have defined a variable about DECL command

i write my name in this variable

 

DECL CHAR ATEC_VAR[10]

ATEC_VAR[1]="benjamin"

 

i read at next location the variable with "while" command

PS read  two quotation marks in variable  ( " "benjamin" " )  see picture

 

error_window.jpg

robot logic.jpg

 

problem nr 2:

 

same situation as problem nr 1

DECL ...

 

i read the variable in the "# Reltool ATEC_VAR[1] " function

ps dosen't read the topic of the variable

 

error_window_reltool.jpg

 

 

Kind regards,

Benjamin Voelzke
4 REPLIES

Re: question about process simulate logic in simulation layer ( DECL CHAR ATEC-VAR[10] )

Siemens Phenom Siemens Phenom
Siemens Phenom

Variables of type strings are, in general, not supported.

 

However for the while, you should write:

WHILE ATEC_VAR[1] = "benjamin"

which is also the correct KUKA syntax and it should work as expected.

 

I do not see the point to use # MoveRelTool ATEC_VAR[1]?

Instead you should have real variables x, y, z and use them in your # MoveRelTool statement.

 

 

Re: question about process simulate logic in simulation layer ( DECL CHAR ATEC-VAR[10] )

Gears Phenom Gears Phenom
Gears Phenom

my request:

 

this is what i want to do

ATEC_VA[1] = "benjamin"

 

# MoveRelTool benjamin X Y Z

 

and the varaible "benjamin" this should be the name of location

 

 

the "while" problem was my fault

thanks

normaly krc syntax  WHILE INPUT > 0     

whitout " " "

Kind regards,

Benjamin Voelzke

Re: question about process simulate logic in simulation layer ( DECL CHAR ATEC-VAR[10] )

Siemens Phenom Siemens Phenom
Siemens Phenom

For MoveRelTool, you need to specify X, Y and Z. You cannot just specify X as you did in your example, that is why you get this syntax error message.

 

Anyway, passing a string variable as MoveRelTool reference location is not supported.

 

You may instead want to use a Custom XML Olp Command in which you will type this reference location name in the creation UI, and use it in the MoveRelTool withing the simulation layer.

 

Re: question about process simulate logic in simulation layer ( DECL CHAR ATEC-VAR[10] )

Gears Phenom Gears Phenom
Gears Phenom

thanks

 

i found a other solutution

 

i work with "txobject" commands in custom xml

 

txobject = location

 

# MoveReltool location X Y Z

 

in this way is working

Kind regards,

Benjamin Voelzke