Cancel
Showing results for 
Search instead for 
Did you mean: 

robot expert missing function

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

i tested robot expert verion 12.1 but i miss important functions.

 

- Mirror

- auto create sweep volume with inference zone

- Dual arm robots

- define component type

- MPA

 

it is possible to implemented these function?

Kind regards,

Benjamin Voelzke
2 REPLIES 2

Re: robot expert missing function

Siemens Genius Siemens Genius
Siemens Genius

Hello Benjamin,

RobotExpert is a different product than Process Simulate that was developed in order to support industries, use cases, workflows and needs that are different than Process Simulate. This is why there is no 1:1 match between RobotExpert and Process Simulate. BTW, there are many more functions that exist in Process Simulate and are missing from RobotExpert and there are commands in RobotExpert that do not exist in Process Simulate. 

There is no plan to add the functions you mention to RobotExpert.

What workflows are you interested in and for which industries? As an example, classic auto biw use cases cannot be completed in RobotExpert, but general arc welding processes are good fit to RobotExpert.

 

Regards,

Gil.

Re: robot expert missing function

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

hello,

 

i can understand robot expert is not the same software.

but i think in robot expert is missing important basic functions.

 

Mirror of paths

auto create sweep volumes

relations viewer

define component type

 

these function i think is basic.

 

thanks