Cancel
Showing results for 
Search instead for 
Did you mean: 

robot signals in robot moduls with array

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

 

in most of robot programs runs logic with arrays

 

currently process simulate can not work with arrays

 

$OUT[O_TCH_COVER_OPEN[ST_NR]]=TRUE

 

example from robot program:

GLOBAL DEF TCH_COVER_OPEN(ST_NR :IN)
INT ST_NR,HANDLE

$OUT[O_TCH_COVER_CLOSE[ST_NR]]=FALSE
$OUT[O_TCH_COVER_OPEN[ST_NR]]=TRUE

 

is there a chance???

 

Kind regards,

Benjamin Voelzke
22 REPLIES

Re: robot signals in robot moduls with array

Siemens Phenom Siemens Phenom
Siemens Phenom

ST_NR=1

O_TCH_COVER_CLOSE[ST_NR]=2

$OUT[O_TCH_COVER_CLOSE[ST_NR]]=TRUE

 

should already work.

Re: robot signals in robot moduls with array

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

GLOBAL DEF PKlappeAuf(BHF_NR : IN)      

DECL INT BHF_NR
 
WHILE (BHF_NR<1) OR (BHF_NR>16)
   WAiT SEC 0.1 ; ungueltige Bahnhofsnummer
ENDWHILE

$OUT[ABDECKUNG_CLOSE_DATA[BHF_NR].AB_CL_NR]=FALSE         
$OUT[ABDECKUNG_OPEN_DATA[BHF_NR].AB_OP_NR]=TRUE

WAIT FOR $IN[ABDECKUNG_OPEN_DATA[BHF_NR].AB_OP_NR]     
WAIT FOR NOT $IN[ABDECKUNG_CLOSE_DATA[BHF_NR].AB_CL_NR]        
$OUT[ABDECKUNG_OPEN_DATA[BHF_NR].AB_OP_NR]=FALSE

END    
    

 

sorry this modul is dosen't work with process simulate

ps writes in simulation layer "$OUT[ABDECKUNG_OPEN_DATA[BHF_NR].AB_OP_NR]" signal not found

Kind regards,

Benjamin Voelzke

Re: robot signals in robot moduls with array

Siemens Phenom Siemens Phenom
Siemens Phenom

This also works:

 

ABDECKUNG_OPEN_DATA[3].AB_OP_NR=1

 

BHF_NR=3

 

$OUT[ABDECKUNG_OPEN_DATA[BHF_NR].AB_OP_NR]=TRUE

 

You need to have ABDECKUNG_OPEN_DATA[BHF_NR].AB_OP_NR defined somewhere, as a variable assignment (reading record/structure definition is not supported).

Re: robot signals in robot moduls with array

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

hello,

 

i have checked the functionality in cee mode

these are the results of the log window

the marked lines show that the function is not executed correctly

 

 

kr360_3[RRS]> Hinweis an home1: [DBG] PKlappeAuf (2)
kr360_3[RRS]> Hinweis an home1: [DBG] Simulate PKlappeAuf (2)
kr360_3[RRS]> Hinweis an home1: [DBG] Simulations Roboter Modul Prozedur PKlappeAuf
kr360_3[RRS]> Hinweis an home1: [DBG] # NotifyCallFunctionExecutionStarted PKlappeAuf
kr360_3[RRS]> Hinweis an home1: [DBG] DECL INT BHF_NR
kr360_3[RRS]> Hinweis an home1: [DBG] $OUT[ABDECKUNG_CLOSE_DATA[BHF_NR].AB_CL_NR]=FALSE
kr360_3[RRS]> Hinweis an home1: [DBG] Evaluate signal ABDECKUNG_CLOSE_DATA[2].AB_CL_NR: 0
kr360_3[RRS]> Hinweis an home1: [DBG] Simulate $OUT[ABDECKUNG_CLOSE_DATA[BHF_NR].AB_CL_NR]=FALSE
kr360_3[RRS]> Hinweis an home1: [DBG] # waittime 2
kr360_3[RRS]> Hinweis an home1: [DBG] Wartezeit: 2 s
kr360_3[RRS]> Hinweis an home1: [DBG] NotifySimulationEvent WaitTime : ON (6,87600000239908ms)
kr360_3[RRS]> Hinweis an home1: [DBG] OnTimeReached : 8,87600000239908
kr360_3[RRS]> Hinweis an home1: [DBG] NotifySimulationEvent WaitTime : OFF (8,87600000239908ms)
kr360_3[RRS]> Hinweis an home1: [DBG] $OUT[ABDECKUNG_OPEN_DATA[BHF_NR].AB_OP_NR]=TRUE
kr360_3[RRS]> Hinweis an home1: [DBG] Evaluate signal ABDECKUNG_OPEN_DATA[2].AB_OP_NR: 0
kr360_3[RRS]> Hinweis an home1: [DBG] Simulate $OUT[ABDECKUNG_OPEN_DATA[BHF_NR].AB_OP_NR]=TRUE
kr360_3[RRS]> Hinweis an home1: [DBG] # waittime 2
kr360_3[RRS]> Hinweis an home1: [DBG] Wartezeit: 2 s

 

 

Kind regards,

Benjamin Voelzke

Re: robot signals in robot moduls with array

Siemens Phenom Siemens Phenom
Siemens Phenom

>> Evaluate signal ABDECKUNG_CLOSE_DATA[2].AB_CL_NR: 0

 

This means you are missing the definition, somewhere before:

ABDECKUNG_CLOSE_DATA[2].AB_CL_NR = <value>

 

As I wrote earlier, you need this assignment to be defined somewhere to have it work. ABDECKUNG_CLOSE_DATA is an array of structures (with fields such as AB_CL_NR). Arrays of structured data are not supported, but you can cheat the system by instead defining the full variable "ABDECKUNG_CLOSE_DATA[2].AB_CL_NR", as it was just a variable name with some special characters (such as [, ] and .) inside.

 

I hope this helps.

Re: robot signals in robot moduls with array

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

sorry i don't understand what you mean.

i have created the signal on robot signals (see picture)

in path editor i call the function (with transfer parameters)

the signals are always connected to logic resource

 

bild1.jpg

 

 

 

bild2.jpg

 

 

bild3.jpg

Kind regards,

Benjamin Voelzke

Re: robot signals in robot moduls with array

Siemens Phenom Siemens Phenom
Siemens Phenom

ABDECKUNG_CLOSE_DATA[2].AB_CL_NR is not a signal name but a signal index.

 

My idea was that you would:

  1) define" $IN[3]" as robot signal

  2) have somewhere instruction "ABDECKUNG_CLOSE_DATA[2].AB_CL_NR = 3" (just an example) before reaching the attempt to send/wait for $IN[ABDECKUNG_CLOSE_DATA[2].AB_CL_NR] signal

This would be aligned with what the actual Kuka controller is doing.

 

Another option could be to define "$IN[ABDECKUNG_CLOSE_DATA[2].AB_CL_NR]" as robot signal. I am not sure it will work but it might worth trying.

Re: robot signals in robot moduls with array

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

the first idea is dosn't work

i have written an instruction "ABDECKUNG_CLOSE_DATA[2].AB_CL_NR = 3" somewhere in robot path

the signal "ABDECKUNG_CLOSE_DATA[2].AB_CL_NR" is always "true" (see at simulation panel)

 

 

second idea is also dosn't work

 

i have created "$OUT[ABDECKUNG_CLOSE_DATA[2].AB_CL_NR]" as robot signal

ps dosn't find the signal

 

Smiley Sad

 

 

Kind regards,

Benjamin Voelzke

Re: robot signals in robot moduls with array

Siemens Phenom Siemens Phenom
Siemens Phenom

In the first idea (which I tested successfully), the signal that should be defined on the robot on Process Simulate is "$IN[3]" or '$OUT[3]", not ABDECKUNG_CLOSE_DATA[2].AB_CL_NR (which is an index - a variable - and not a signal).

 

I will check the second idea.