Cancel
Showing results for 
Search instead for 
Did you mean: 

select speed paramter in path template

Gears Phenom Gears Phenom
Gears Phenom

hi,

 

is it possible to select speed or zone parameter from normal via location (kuka krc) in path template?

 

in normal way i can write a new value for zone or speed data via path template xml.

but this value is fix.

 

is it possible to select in path template window the speed or zone value?

 

thanks

Kind regards,

Benjamin Voelzke
5 REPLIES

Re: select speed paramter in path template

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi,

 

IMHO: it is not possible.

 

David

Re: select speed paramter in path template

Siemens Phenom Siemens Phenom
Siemens Phenom

I also think it is not possible to get a list from the controller (same list as you see in Path Editor). It is worth opening an ER...

Re: select speed paramter in path template

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

I don’t know your problem in detail, but try to use a workaround – set a flag as a OLP command in the Path Editor –in Path Template then switch the code according this flag. Not so elegant, but still helpful.

 

David

Re: select speed paramter in path template

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hello again,

 

is this what you are searching for? Tested on the PS 13.0

 

 path_template_set_param_1.jpg

 

 

path_template_set_param_2.jpg

Re: select speed paramter in path template

Legend
Legend

Hello, voelzke!

 

Can you detail a bit more about what you're trying to achieve or the problem you're trying to solve?

 

If you're trying to multi-edit those values, you can do it using "Set Location Properties" in Path Editor tab. If those parameters are not enabled for editing you'll need to modify your path editor columns xml (here located at C:\ProgramData\Tecnomatix\Process Simulate\12.1.3\Robotics\PathEditor\AvailableColumns).

 

If you need info about the xml modification, please let me know

 

Regards,