Cancel
Showing results for 
Search instead for 
Did you mean: 

transport a internat rob signal from motion parameters to olp parameters

Gears Phenom Gears Phenom
Gears Phenom

hello,

 

i search a solution for transport a internat rob signal from motion parameters to olp parameters.

INFO! In PS Standard Mode not Line Simulation

 

My Way:

I will write in all Move Locations the actual position number.

in OLP logic i will work with the actual position number. (call sub routine)

 

i can't read or work with the olp variable in my test senario.

Kind regards,

Benjamin Voelzke
1 REPLY

Re: transport a internat rob signal from motion parameters to olp parameters

Siemens Phenom Siemens Phenom
Siemens Phenom

By internal rob signals, do you mean "variables"?

 

I understand you want to use parameters set on the customized location in the Olp Commands afterwards. In this case you use:

# SetVariable MyVar <motionParameter>

in the simulation layer of the customized location.

Then the variable MyVar will be global and known by the simulation and can be used in the simulation layers of the next Olp Commands.

 

Is it what you are looking for?