Airborne Noise Transmission Analysis

Experimenter
Experimenter

How do i setup the online processing tab of signature acquisition to analyse an FRF to get information about airborne noise transmission. i know it can be done with add-ins but i do not have enough tokens for that.

2 REPLIES 2

Re: Airborne Noise Transmission Analysis

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

You do not need any additional add-ins to calculate FRFs and FRF\Coherence in Signature Acquistion on the Online Processing worksheet.  If you need to send a signal out to a Volume Velocity source, for example, then you would need the Source Control add-in which requires 8 tokens.  If needed, you could turn off some other add-ins if they are not needed for this test.

 

Is that what you are asking?

Re: Airborne Noise Transmission Analysis

Experimenter
Experimenter

Yes that helps! Thank you.