Any Way to Have More Than One Curve Per Plot When Using the Batch Printing Feature in Test.Lab?

Experimenter
Experimenter

Hello,

 

I am having trouble figuring out if there is a way to have more than one curve on a plot when using the batch printing feature in Test.Lab Random Control. For example, I would like to have my nominal test level, test tolerances, inline accelerometer, and cross axis accelerometers PSDs all on one plot for easy comparison. However, when I use the tool, the curves are all plotted seperately on their own PSD plot.

 

Thank you in advance,

 

bollinms

1 REPLY 1

Re: Any Way to Have More Than One Curve Per Plot When Using the Batch Printing Feature in Test.Lab?

Siemens Phenom Siemens Phenom
Siemens Phenom

You might want to try the "other" batch printing feature in Testlab:

 

https://community.plm.automation.siemens.com/t5/Testing-Knowledge-Base/LMS-Test-Lab-Batch-Reporting/...

 

You can control grouping in this one.