Cancel
Showing results for 
Search instead for 
Did you mean: 

Batch reporting color for traces...

Creator
Creator

When I use batch reporting for overlays ofetn there may be 3 to 4 runs to overlay when the signature of a unit  is checked. One of the colors is light blue which does not show up well to the user. its the third color. How can I chance the default c olor selection to not use the light blue color? Thx in advance.

1 REPLY

Re: Batch reporting color for traces...

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

this is unrelated to batch reporting.  By default curve 5 in the display is light blue (cyan?).  You have several options available to you to resolve.

 

1)  In Batch Reporting, in the display \ picture you are using right click and go to Options...  Go to Curve Property Schema, turn on "Overrule default curve property schema".  Go to Edit... and change the schema for curve 5 and any other curves you wish.   Under File, Printing Options make sure that under General Settings, User picture settings from Test.Lab Pictures or Pictures in the print format, except curve properties.  That will modify this one picture and use it's curve property schema when printing.

 

2)  In the PrintFormat used for the Batch Reporting, within MS Word or MS PowerPoint, edit the format such that in the display \ picture you are using right click and go to Options...  Go to Curve Property Schema, turn on "Overrule default curve property schema".  Go to Edit... and change the schema for curve 5 and any other curves you wish.     In this case, under File, Printing Options make sure that under General Settings, User picture settings from Pictures in the print format.  That will modify your print format so that whenever it is used the curve properties and look of the picture remain the same.

 

3)  You can globally change the curve property schema in Test.Lab, under Tools, Options, Displays Change... the default property schema.  Change the schema for curve 5 and any other curves you wish.     Under File, Printing Options make sure that under General Settings, User picture settings from Test.Lab Pictures or Pictures in the print format, except curve properties.the print format.  That will modify all of your 2D pictures to use this curve property schema.