Cancel
Showing results for 
Search instead for 
Did you mean: 

CAN bus sampling rate same as vibration sampling rate?

Experimenter
Experimenter

I am using LMS Test.Lab Signature.  I want my CAN bus channels to have the same sampling rate as my vibration channels.  Is there a way to do this?  CAN static sampling rates are 100, 200, 400, etc.

2 REPLIES 2
Highlighted

Re: CAN sampling rate same as vibration sampling rate?

Siemens Phenom Siemens Phenom
Siemens Phenom

Try changing the CAN bandwidth from 'Static' to 'Vibration' in the upper right corner of the Acquisition Setup worksheet:

 

can_static.png

 

 

 

Re: CAN sampling rate same as vibration sampling rate?

Experimenter
Experimenter

Thanks, that worked!