Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't create SmartScope template from LMS Test.Lab

Creator
Creator

Trying to make a SmartScope template from LMS Test.Lab 16A.  "Save standalone recording template..." is grayed out under "File".  Picture below.

 

mag.png

 

Under Tools -> Add-ins, the add-in 'Standalone recording' is turned on. 

 

 

 

 

 

3 REPLIES 3

Re: Can't create SmartScope template from LMS Test.Lab

Experimenter
Experimenter

try to create the template form the "measure"-workbook. Not form the "channel setup"-workbook.

Re: Can't create SmartScope template from LMS Test.Lab

Siemens Phenom Siemens Phenom
Siemens Phenom

The Navigator worksheek will allow you to write the template as well.  Some worksheets (Channel Setup, Acquisition Setup and Tracking Setup) will show that option as insenstive (greyed out).  I believe the reaon is that settings can changed on those worksheets.  By moving to another worksheet like the Navigator (where no settings can be changed) you can then save the Standalone Recording template.

Re: Can't create SmartScope template from LMS Test.Lab

Creator
Creator

That worked! Thanks