Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Can't view Canbus channels in LMS Smartscope?

Creator
Creator

Created a standalone template from LMS Test.Lab in a project with a DBC file where I can see and record canbus channels.

 

Put the standalone template onto ScadasXS flash drive.  In Measurement Setup of Smartscope, can see all Canbus channels listed under CAN tab.

 

But when I acquire, I don't see those Canbus channels anywhere.  Can't display them, see them, or nothing.

 

What gives? Any ideas?

3 REPLIES 3

Re: Can't view Canbus channels in LMS Smartscope?

Siemens Legend Siemens Legend
Siemens Legend

Hi,

Have you import the template from the SD card to flash memory?  If you're, you can select the template->edit->CAN, in CAN setup screen upper right corner->CAN VISUALIZAION, you can turn on view the canbus channels during data acquistion and offline processing too.

Here's a picture:

CAN.jpg

Hong

Re: Can't view Canbus channels in LMS Smartscope?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

CAN Visualization is offered from SmartScope Version 4.0 and later.

 

The CAN signals to be monitored in the displays can be selected after tapping on CAN VISUALIZATION. The selection is done at CAN message level: all signals which are part of the selected message will be available for visualization. see attached doc file.

 

 

Re: Can't view Canbus channels in LMS Smartscope?

Creator
Creator

Thanks.  It was "CAN Visualization" at the top of the screen that did the trick to make the Can channels visible.