Cancel
Showing results for 
Search instead for 
Did you mean: 

Connect Scadas III (316) with Scadas Mobile as MAster-Slave

Creator
Creator

Gents,

 

We need to perform an acquisition and to fulfill the total amount of channels needed we would need to connect the Scadas III (master) with a Scadas Mobile (would be as Slave). I have make it in the past with Scadas III racks, but Is it possible to do it with the two mentioned technologies?

 

Thanks in advance

 

Francisco Climent

Autoneum

1 REPLY 1

Re: Connect Scadas III (316) with Scadas Mobile as MAster-Slave

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Francisco,

 

Unfortunately this is not possible.  The Scadas III hardware can only work as Master / Slave with other Scadas III hardware.


The Scadas Mobile / Recorder and the Scadas Lab frames can Master / Slave with each other but not with the older Scadas III hardware.

 

For more information see this FAQ on the GTAC site:  https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&q=slave&dt=faq&pd=lms-t...