Copy sections between LMS Test.Lab projects?

Creator
Creator

A quick question for the day. I want to copy a few sections with processed data from one project to another. What is the best way to do that?

2 REPLIES 2

Re: Copy sections between LMS Test.Lab projects?

Siemens Phenom Siemens Phenom
Siemens Phenom
  1. Open the project you want to copy the sections into (in 1st picture below it is “Project2”)
  2. Under “My computer” navigate to the project you wish to copy the sections from (in 1st picture below this is “Stereo”).
  3. Highlight the project name ("Stereo") on the navigator on the right side navigation tree.
  4. Highlight the sections you wish to copy in the middle pane.  Multiple sections can be selected using “Shift” or “CTRL” keys.
  5. Right click and select “Copy”.
  6. Right click on destination project ("Project2") on right side and select “Paste” (2nd picture).
  7. Sections will be copied.
  8. section_copy.pngPicture 1: Highlight project that sections will copied from on right, and select sections to be copied in middle pane

     section_copy2.pngPicture 2: Right click on destination project and pick "Paste"

     

 

 

 

 

 

Highlighted

Re: Copy sections between LMS Test.Lab projects?

Siemens Phenom Siemens Phenom
Siemens Phenom

PJS's suggestion works fine.  Another option in the LMS Test.Lab Desktop would be to open both projects at the same time and then Tile them via Window, Tile.  You can then copy and paste from one project to the other since they are both open.