Cancel
Showing results for 
Search instead for 
Did you mean: 

Create run names for data calculator results

Experimenter
Experimenter

Is there a possibility to create a run name for the results of the data calculator?

 

When you create a new block as the result of a calculation in the data calculator and you want to display it together with other blocks from measurements you get a problem when you use the section/name and run/name for the legends. You can give this result a section name by saving it into a section with teh appropriate name but the field for the run man will stay empty.

Edit properties don't work here and creating a sub-folder in the section by create folder and save the new block here dosn't work either.

Example Legend.JPG

2 REPLIES

Re: Create run names for data calculator results

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,  I see two fairly simple options:

 

1)  When using Save Results As... save to any previously saved run.  The saved results will then have that run name.

2)  Copy and Paste a run to the section thus create Run 1 (1) or similar, edit the run name to whatever you want, delete the data that exists and Save Results As... to that new run.  Or if already saved, copy the results to the new run.

 

 

Re: Create run names for data calculator results

Experimenter
Experimenter

Hello Kevin,

 

thank you very much, option 2 works good for me.

A bit awkward all this copy and rename but it works.Smiley Happy