Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

How do I apply the ISO Wk and Wd weighting?

Experimenter
Experimenter

Have vibration spectral data in LMS Test.Lab.  Can I apply the ISO weighting filters (Wk and Wd)?

1 REPLY 1

Re: How do I apply the ISO Wk and Wd weighting?

Siemens Phenom Siemens Phenom
Siemens Phenom

The ISO 2631 Whole-Body vibration filters Wk (vertical) and Wd (horizontal) can be applied by right clicking on the Y-axis of the vibration spectrum display.

 

wk.png

 

Right click and choose "Processing -> Weighting/More -> Wk or Wd".

 

This is possible from Testlab Revision 18 and higher.

 

If wanting to filter time domain data, under "Tools -> Add-ins" turn on "Human Body Vibration".

 

addin.png

 

In the Time Signal Calculator, a new function called FILTER_ISO2631 is added to the list of available functions.

 

filter.png

 

It can be used to filter time histories.