In Simcenter Testlab Neo, process has warning symbols

Creator
Creator

Went to run Simcenter Testlab Neo process today, but I cannot.  The process steps have a warning symbol through them like this:

 

warning.png

Any ideas?  Was working yesterday.

3 REPLIES 3

Re: In Simcenter Testlab Neo, process has warning symbols

Siemens Phenom Siemens Phenom
Siemens Phenom

Looks like some of the add-ins used to create the process were turned off.   Under "File -> Add-ins" in Simcenter Testlab Neo, turn on the following add-ins:

  • Load Data Analysis
  • Fatigue Life Analysis
  • Interactive Analysis

 

addin.png

 

Re: In Simcenter Testlab Neo, process has warning symbols

Creator
Creator

Thanks, that worked!

 

work.png

 

I recently got a new PC and reinstalled the software, so probably lost the add-ins that way.

Highlighted

Re: In Simcenter Testlab Neo, process has warning symbols

Siemens Phenom Siemens Phenom
Siemens Phenom

Also, if you are unsure what licenses or add-ins you need to load, hovering over the red error box on the method will show you what license or add-in is required for that method.  See the Licensing message in the popup below:

 

2019-08-07 13_49_55-Simcenter Testlab Desktop Neo - Project1 - Section1.jpg