Cancel
Showing results for 
Search instead for 
Did you mean: 

Installation of Active Pictures plug-in

Experimenter
Experimenter

Hello,

 

I am trying to install the Active Pictures plug-in (14A or 15A) but I am facing the error message in the picture attached.

The install log file indicates that the issue is linked with the script: FilePatternReplacerASAM_ODS_Corba2.vbs

Any idea what could be causing this or how can I go around this?

 

I tried both the versions on 2 different computers and faced the same error.

 

Thank you ....

 

Rabah

 

2 REPLIES

Re: Installation of Active Pictures plug-in

Siemens Experimenter Siemens Experimenter
Siemens Experimenter
One thing to try is right click the installation and run as administrator. Also make sure the operating system you are installing the 14A and 15A on is newer than Windows XP. The 14A release was the first revision where Windows XP support ended.

Re: Installation of Active Pictures plug-in

Experimenter
Experimenter

Run as Admin got me around it.

Thank you !