Cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to lockdown a test?

Creator
Creator

Is it possible to lockdown a test?  I want to create a test template that the test cell operators cannot change the frequency resolution, as well as the tracking settings.  Using LMS Test.Lab Signature.

2 REPLIES 2
Highlighted

Re: Is it possible to lockdown a test?

Siemens Genius Siemens Genius
Siemens Genius

there is a possiblity through the Add-in "Parameter locking".

see document in attach for more info

Re: Is it possible to lockdown a test?

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, you can do this using “Parameter Locking”.  Have the project/template open that you want to use, with all add-ins needed turned on. Here are the steps:

 

  • In Signature, go to Tools -> Add-ins and select “Parameter Locking”.  Click “OK” on the message “By selecting the Add-in Parameter Locking field….”. Press “OK” on the add-in menu.

 

  • To lock the frequency resolution, go to the Acquisition Setup worksheet.  Right click on the frequency resolution and choose “Property Dialog”.

property_dialog.png

 

 

  • A “Combobox” property dialog will open up.  In the dialog box, check on the “Read Only” field and press OK.

combo.png

 

Now the frequency resolution field cannot be changed.  You can do the same in the Tracking settings worksheet as well. Save the template or project and send to the test cell operator!