Cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to use a NI DAQ System with the LMS Test.Xpress Software?

Creator
Creator

Good Afternoon People!!

 

I'm Alvaro and I'm working with LMS Test.Xpress. It's very good software!.

 

I'm only have a question for the moment. It's possible to use a NI DAQ System with the LMS Test.Xpress Software? How to do it? thanks for the answers..

 

Grettings.

Alvaro

7 REPLIES

Re: LMS Test.Lab Signature

Siemens Legend Siemens Legend
Siemens Legend

Hello Alvaro,

 

LMS Test.Xpress software cannot works with National Instruments Data Acquistion system.  Test.Xpress works with our SCADAS frontend hardware.

LMS Test.Lab can import NI Diadem file and analyze the data.

 

Hong

Re: LMS Test.Lab Signature

Creator
Creator

Thanks for the Information friend! 

 

Really these softwares have many interesting functions, I'm very interested in learn more about LMS Test.Lab and Test.Xpress, again thank you very much. I hope to resolve some doubts more in the future about this subject.

 

Greetings.

Alvaro

Re: LMS Test.Lab Signature

Experimenter
Experimenter

Dear expert,

 

What's the DIAdem file format?

The NI data format is .tdms.   Lms can not read it  directly.  

 

BR.

HeChe

Highlighted

Re: LMS Test.Lab Signature

Creator
Creator

LMS Test.Lab can read .TDMS File? I guess can't.

 

Help with my doubt please.

 

Grettings

Alvaro 

Re: LMS Test.Lab Signature

Experimenter
Experimenter

Yes, you can not use the .tdms file directly.

I change the format to .uff file .  it's perfect avialble.

Re: LMS Test.Lab Signature

Creator
Creator

I can use TDMS files in the Lms Testlab.  Just turn on "Durability Drivers Pack" under "Tools -> add-ins".  I can browse to and use TDMS files.

 

ni_addin.png

 

 

 

Re: LMS Test.Lab Signature

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, SLars is correct.  The TDMS format is included with the Durability Driver's Pack Add-In.

 

For revision 14A and earlier this license had to be purchased and the Add-In turned on.

 

For revisions 15A, 16A and 17  this is included with the Desktop.  You still need to turn the add-in on, but no extra license is required.

 

For revision 18 and later the add-ins are not required for any of the data drivers, so for the durability file types, Nastran, Ansys, DATx, Excel, etc. just browse to the files via My Computer to plot them, add to input basket, etc.