cancel
Showing results for 
Search instead for 
Did you mean: 

LMS Test.Lab Order Tracking question

Creator
Creator

I’ve been trying out the order tracking add-in in LMS Test.Lab and have a question.  Is there a way in the online processing worksheet to set the order tracking parameters (max order and order resolution)?  Those appear to be fixed at max order 32 and resolution 0.25 order.  These can be readily changed in time data processing, but I’d like the same options in online processing.

1 REPLY

Re: LMS Test.Lab Order Tracking question

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

You can change the settings for online order tracking in LMS Test.Lab Signature:

 

  1. Go to ‘Measure’ worksheet
  2. Select the ‘Acquisition’ tab (F5) in the upper right
  3. Choose the OT tab (F11) in the middle right
  4. Set the Max order, order resolution, etc as desired

ot.png