Highlighted

LMS Test.Lab - Save more frontback as picture all together

Pioneer
Pioneer

Hi,

i created more frontback on Test.Lab and i need to insert all in a powerpoint presentation.

Is it possible to save as picture everyone with one command?

 

 

Thank you

4 REPLIES 4

Re: LMS Test.Lab - Save more frontback as picture all together

Siemens Phenom Siemens Phenom
Siemens Phenom

Try the following to print all pictures into Powerpoint with one command:

 

1.  In Testlab, choose "File -> Printing Options".  Set Office application to Powerpoint and set the mode to Electronic rather than paper.

printing_options.png

2.  Then choose "File -> Print" from the main menu.  A prompt will appear for the directory and name for the powerpoint file to be created in.

print.png

 

3.  In the powerpoint, each picture layout (frontback, colormap, etc) is one page in the resulting powerpoint. 

one_page_per_layout.png

 

To control the appearance in powerpoint (add logo, change size) see Testlab Format based printing with Powerpoint knowledge base article.

 

Hope that helps!

Re: LMS Test.Lab - Save more frontback as picture all together

Pioneer
Pioneer

Thank you!!

Re: LMS Test.Lab - Save more frontback as picture all together

Siemens Phenom Siemens Phenom
Siemens Phenom

One quick tip when doing the format based printing.  After generating the format with the "Make Printformat...", be sure to remove the current data from the format (right click and remove the data).

 

If you don't, your format will have data in it already, and any new data will be plotted on top of it.  Best to have a clean empty format.  Screenshot below.

power.png

 

Re: LMS Test.Lab - Save more frontback as picture all together

Pioneer
Pioneer

Thanks!