Cancel
Showing results for 
Search instead for 
Did you mean: 

LMS Test.Lab Strain Gauge instrument modal analysis

Experimenter
Experimenter

Hi!

 

I would like to know if somebody has experience in Modal Analysis with data measured by using strain gauges running Test.Lab.

Do I have to pre-process my data to use Test.Lab modal analysis packages?

My main goal is to compare the modal analysis performed with accelerometers vs. that performed with strain gauges.

 

Thanks for any help yo may provide.

 

1 REPLY

Re: LMS Test.Lab Strain Gauge instrument modal analysis

Creator
Creator

Basically the only thing to consider is that you are giving displacement data for creating yout mathematical model. With the strain gauges you measure uSt, and you should convert it to absolute displacement. Best would be to acquire only the dynamic part of the strain signal in order to use the full ADC range and have the best resolution. Then yor FRFs will be microns/N instead m/s2/N... but the modal parameters can be calculated.

 

Be aware that the dynamic response of the Strain gauges is much more limited than an accelerometer. I mean, the reliability of the measurement is much more limited in frequency. But if you are considering Strain Gauges is probably beacuse your frequency range is for sure low.