Cancel
Showing results for 
Search instead for 
Did you mean: 

LMS Testlab active picture: How do I copy data from an active picture into LMS Test.Lab?

Creator
Creator

I have data in an active picture in powerpoint that I want to put in LMS Test.Lab.  I lost the original project file. How can I get the data out of my active picture and back into LMS Test.Lab so I can plot it with some new data?

6 REPLIES 6

Re: LMS Testlab active picture: How do I copy data from an active picture into LMS Test.Lab?

Siemens Phenom Siemens Phenom
Siemens Phenom

I have data in an active picture in powerpoint that I want to put in LMS Test.Lab.  I lost the original project file. How can I get the data out of my active picture and back into LMS Test.Lab so I can plot it with some new data.

cop.png

 

Paste the data into a new Excel workbook and save it to a directory.

exc.png

 

 

In LMS Test.Lab, under “Tools -> Add-ins” select “Excel Data Driver”.

add.png

 

Then in the LMS Test.Lab Navigator, drill into the directory with the Excel file.  Select the worksheet and then the measurement, just as if it was LMS Test.Lab native data.  The data can be dragged into a display.

drag.png

 

The data can be plotted and processed directly fromt the Excel file.  If you want, you can also copy and paste the data from the Excel file into the active project.  Just right click on the data and select "Copy", and go to a folder and/or section in the active project and right click "Paste".

 

Hope that helps!

Re: LMS Testlab active picture: How do I copy data from an active picture into LMS Test.Lab?

Creator
Creator

Thank you for the prompt reply.  That worked for me.

Re: LMS Testlab active picture: How do I copy data from an active picture into LMS Test.Lab?

Experimenter
Experimenter

I'm running Active Pictures version 17.1 and the "Copy Values" options are both greyed out - even after selecting the curve.  

Re: LMS Testlab active picture: How do I copy data from an active picture into LMS Test.Lab?

Siemens Legend Siemens Legend
Siemens Legend

can you share the active picture in power point here?

Hong

Re: LMS Testlab active picture: How do I copy data from an active picture into LMS Test.Lab?

Experimenter
Experimenter

Sure - if you could explain how to do that.

Re: LMS Testlab active picture: How do I copy data from an active picture into LMS Test.Lab?

Siemens Legend Siemens Legend
Siemens Legend

Here's the link to explain how to create active picture in Test.Lab: https://community.plm.automation.siemens.com/t5/Testing-Knowledge-Base/LMS-Test-Lab-Active-Picture/t...

 

Hong