Cancel
Showing results for 
Search instead for 
Did you mean: 

Modal analysis

Pioneer
Pioneer

Hi, 
How we can choose the order of the modal in order to obtain the stabilization diagram ? 
Than how can we choose poles.
For example, in this stabilization diagram, I find difficulty to select poles.



 

FRF1.png

 

 

 Thank you
Asia

 

 

 

6 REPLIES

Re: Modal analysis

Siemens Legend Siemens Legend
Siemens Legend

The stabilization diagram you provided, there aren't any stable pole "S".  Here I upload a picture to explain what O, F, D, V & S mean on the diagram, you want to select the pole where it has  "S", both frequency, dampling and vectors are stable within the tolerance.

Picture1.jpg

You can find this information by clicking the question mark on the upper right hand corner of the Stabilization minor worksheet.  I would look at the integrity of all the FRFs measurement you acquired, and look at the coherence of each one.  If the coherence is bad, the FRF might not be any good.

 

Good Luck.

Hong

 

Re: Modal analysis

Pioneer
Pioneer

First thank your for your response .
These are all the FRF mesured and the sum of them:

 10.png

 

And this is the stabilization diagram:

 11.png

 

 For the coherence function, they are no saved in my project.

Re: Modal analysis

Siemens Legend Siemens Legend
Siemens Legend

You should always saved the coherence function in impact testing.  Ideally where there's a resonance(Peak in the the FRF), you would like the coherence close to one; it indicate the relationship between the output(accelerometer) vs input(hammer), when it's close to one that mean the energy input by hammer is excite the structure and responde is contribute by the input, and when the coherence is low, that mean there's energy loss due to some other contraint or could be anti-resonance.

 

How big is the structure you're measuring?  Can you use more accelerometers?  You might not have enough data(FRFs) to analyze the structure.

Picture3.jpg

 

In addition what you're already select to display, you should select MIF/Imaginary Sum then there are more options from the drop down menu, these are different type of Mode Indicator Functions(MIF):

Picture4.jpg

 

again you can find the information by going the question mark on the upper right hand corner in any of the modal analysis workbook you're in.

 

Hong

 

Re: Modal analysis

Creator
Creator

Have you considered using the Polymax Curvefitter rather than the Time MDOF curvefitter?

 

Here is a picture of the difference in the stabilization diagram for the same set of FRFs:

time_vs_poly.png

 

 A little easier to interpret the Polymax curvefitter results.

 

 

Re: Modal analysis

Creator
Creator

Which kind of structure are you characterizing? Which is the frequency range of interest?

It seems that you have issues with you FRFs, did yout confire the windowing properly? And the pretrigger? The ranges were adjusted? What is the S/N ratio?

 

If all the previous is correct, it seems that you are getting very low responses (very big structure? ,close to other noise sources (machines operating nearby)??

If you get a good FRF set, you can use Time MDOF without any troubles.

Re: Modal analysis

Pioneer
Pioneer

Yes,
when I tried with the polymax method, results are better.12.png

 

Thank you 

 

Asia