Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Not a Rundown?

Experimenter
Experimenter

Sorry for troubling, I must be doing something wrong.

 

I have rundown data that I am plotting that always looks like a runup (see below).

 

I went from 3000 RPM to 1400 RPM but it always plots 1400 RPM to 3000 RPM.

 

rundown.png

 

 

 

2 REPLIES 2

Re: Not a Rundown?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

The tracking axis, the X axis in a 2D display and Z axis in a waterfall and colormap, has always been shown in increasing order for run ups and rundowns.  This has changed in Simcenter Testlab 18 with a new feature.  You can now right click on the tracking axis (X axis in 2D display and Z in waterfall and colormap displays) and select reverse.

 

Here is a slide from a What's New presentation.  You can read what's new in Simcenter Testlab rev18 and view presentations on the new features on the Global Technical Assistance Center (GTAC) under Documentation for Simcenter Testlab.  Here is a link, you can click on the rev18 tab at  the following https://support.industrysoftware.automation.siemens.com/docs/simcenter/simcenter_Testlab/.

 

10-26-2018 7-36-44 AM.jpg10-26-2018 7-38-30 AM.jpg

Re: Not a Rundown?

Experimenter
Experimenter

Thank you so very much Kevin.  This worked for me:

reverse.png