Cancel
Showing results for 
Search instead for 
Did you mean: 

Replace a curve without messing up color?

Experimenter
Experimenter

Put some data in a display, but made a mistake.  Want to replace one of the curves.  

 

After I remove the curves I did not want, and then add new data, the colors are no longer correct. 

1 REPLY 1

Re: Replace a curve without messing up color?

Siemens Phenom Siemens Phenom
Siemens Phenom

Don't remove the curve and then add new data.

 

Instead, drag and drop the correct data over the curve you want to replace in the legend, like shown below:

replace_gif.gif

 

 

This replaces the curve and does not mess up the linestyle colors.

 

You could also try Replace Data Origin feature.