Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Runlogging file opens in Excel rather than notepad...

Creator
Creator

For some reason the runlogging file now wants to open in Excel rather than in Notepad. The Test lab version is 11b. How do i corect this? Thank you.

1 REPLY

Re: Runlogging file opens in Excel rather than notepad...

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Chuck,

 

This works with later versions of LMS Test.Lab, so I assume 11B would behave the same.  I believe you've changed your default program to open *.txt  files with Excel.  If I change the default program to open *.txt files to be excel, I see this behavior.

 

  • Right click on a file with the *.txt extension (or if your runlogging file has a different extension then select that file type) and select Open With.  If you don't see Open With, try Shift-Right Click.
  • Select Open With, Choose default program. 
  • Select Notpad, Wordpad, or whatever text editor you desire AND turn on the option "Always use the selected program to open this kind of file."
  • Test.Lab will now use this program - you don't even need to restart Test.Lab