Cancel
Showing results for 
Search instead for 
Did you mean: 

ScadasXS Binaural headset with ScadasMobile?

Experimenter
Experimenter

We own a binaural headset that we use with our ScadasXS.  Is it possible to use it with our ScadasMobile? If so, how do I plug it in?

headset.jpg

 

 

It is product code SCx-ABH04, I think.

 

3 REPLIES

Re: ScadasXS Binaural headset with ScadasMobile?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Depending on the type of card you have in your SCADAS Mobile, you will need either adapter cable SCX-ABH04-V (LEMO to CAMAC) or SCX-ABH04-B (LEMO to BNC).  Contact your sales representative for a quote.

Re: ScadasXS Binaural headset with ScadasMobile?

Siemens Phenom Siemens Phenom
Siemens Phenom

You can use your ScadasXS headset with a ScadasMobile.  Depending on the acquisition card (VB8-E, V8-E, etc) there are different adaptor cables available.

 

cables.png

 

There is also an adaptor that goes from the lemo connection on the headset to a stereo jack so the headset can be used with a PC.

Re: ScadasXS Binaural headset with ScadasMobile?

Experimenter
Experimenter

Will do.  Thanks for the info!