Should I index? "No valid index file was detected"

Experimenter
Experimenter

Working with Testlab Neo, a very fine product by the way!

 

Sometime I get this message when opening a project:

index.jpg

 What is the correct answer?  Should I say Yes to index the project?  Or No?

 

 

1 REPLY 1

Re: Should I index? "No valid index file was detected"

Siemens Phenom Siemens Phenom
Siemens Phenom

You should say Yes and let the index be created!

 

In Testlab Neo, there is a new feature called a pivot table that lets you access and view all the data in your project very quickly.  To do this fast, the data in the project is already indexed so it can make the table very quickly.

 

If you open a project from Testlab "Classic", the index does not exist already.  So the software asks to create one.  Other than waiting a little while the first time you open the project and index it, it does not affect anything other than making the pivot table faster.  You can still open the project in Testlab Classic afterwards, etc.