Cancel
Showing results for 
Search instead for 
Did you mean: 

SoundBrush Intensity Vectors in Report File

Experimenter
Experimenter

Hello,

I have used the LMS SoundBrush to map 3D sound intensity fields with much success.  I am now attempting to utilize the Report Generating functionality to export the measured data for further processing.  The sound intensity results are easily exported to Excel as shown below.

 

7-12-2018 5-36-59 PM.jpgSound Intensity Results from Soundbrush3

As you can see, the data is arranged in columns, where from left to right we have:

  • Positions (sequential scan index number for each datapoint)
  • Time (Timestamp for each datapoint)
  • Red/Green/Blue (X,Y,Z cartesian coordinates for each data point)
  • Pitch/Yaw angle (I assume this is the direction of the intensity vector)
  • Overall (dB magnitude of the overall intensity vector)
  • 100Hz/125Hz...4000Hz (dB magnitude for each 1/3 octave band intensity vector)

My question is with regard to the Pitch and Yaw.

  1. Am I correct that this is the direction of the intensity vector?
  2. If so, to which frequency does this intensity vector correspond?
  3. Is it possible to export the direction for each 1/3 octave band?

Many thanks!

 

-Nick