Cancel
Showing results for 
Search instead for 
Did you mean: 

Source not working?

Experimenter
Experimenter

A Siemens support engineer told me that my SCADAS Mobile has two built in sources.

 

I went to try and use them and got a error, pictures below:

 

source.png

 

Instead of running my usual Signature, I ran Analog output.  I have tokens, but it would not start.

 

?

 

 

2 REPLIES 2

Re: Source not working?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

No, Analog Output is another product, you don't want that.  Use your normal Signature product and after opening a project, select Tools->Add-ins and turn on Source Contro.  That should add a new dialog in the Acquisition Setup worksheet where you can set up your source output.

Re: Source not working?

Siemens Phenom Siemens Phenom
Siemens Phenom

The source setup in Acquisition Setup will look like below:

 

source.png

 

It is in the lower right area of the Acquisition Setup.