Cancel
Showing results for 
Search instead for 
Did you mean: 

Start LMS Test.Lab Desktop with no project?

Creator
Creator

Is it possible to start the Desktop without a blank project?  I would like it to start like Signature, where no project is opened by default (and there is just a blank screen).

 

1 REPLY 1

Re: Start LMS Test.Lab Desktop with no project?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Right click on the Desktop shortcut and in the Target field, scroll all the way to the end of the command and add -b, it should look like this:

 

"C:\Program Files (x86)\LMS\LMS Test.Lab 17\bin\LmsHq_ProductVC_LmsDesktop_v1.exe" -b