Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

View more that a few seconds of data?

Experimenter
Experimenter

I am taking data with Testlab signature software.  I cannot see more than a few seconds of data at a time.

 

Want to see at least 30 seconds of the signal I am recording....

2 REPLIES 2

Re: View more that a few seconds of data?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

On the Measure worksheet of Signature Acquisition / Signature Testing press the More... button and make sure that Monitoring is on and adjust the History size.  In current versions of the software the default is 2 seconds but can be increased to 300 seconds as a buffer in later releases.  Older releases may have a limit of 30 seconds or 60 sseconds but currently it can be set to larger values.

 

12-7-2018 10-08-22 AM.jpg

Re: View more that a few seconds of data?

Experimenter
Experimenter

Thank you sir, that worked!

 

I did have to drop data from the Time History functions in the Monitor folder into my display to see all the data!

 

time_history.png