Cancel
Showing results for 
Search instead for 
Did you mean: 

Alias Mapping: Matching Geometry to Test Measurement Data

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

 

(view in My Videos)

 

Imagine you've been acquiring vibration data all day... while analyzing, your boss suggests animating an operational deflection shape with the data.

 

The only problem is that you did not use the same naming convention on the geometry as you did with the test data. Or even worse, the data was stored without suitable names and directions for a geometry animation.

 

Previously, if these names did not match, either the geometry names or the data names would have to be altered to match. That’s a lot of renaming just to animate a shape, especially if a lot of different runs and configurations were tested!

 

 

1.pngFigure 1: When the modal data node names and the geometry node names do not match an error is generated: “No matching nodes found – Check alias table”.

 

As of Simcenter Testlab Version 17 and higher, an alias table (similar to a lookup table) has been introduced so that mapping can be done between the geometry and the modal data. This makes it possible to animate shapes without altering node names.  Simcenter Testlab was formerly called LMS Test.Lab.

 

Example of using alias table: modal analysis of a golf club

 

Imagine conducting an impact test on a golf club. Data is taken in the X and Y directions at eleven points along the physical club. FRFs are calculated for all the runs and it is now desired to animate mode shapes in Simcenter Testlab.

 

2.pngFigure 2: A CAD model of the golf club with accelerometers represented with yellow dots. Data was taken in the X and Z directions at all accelerometer locations.

A simple geometry is created in Simcenter Testlab that matches the accelerometer locations on the physical object in Figure 2 above.

3.pngFigure 3: A wireframe geometry of the golf club is created. Each node represents an accelerometer location.

The node names between the geometry and the modal data do not match. Rather than renaming all of the nodes in the geometry or in the data, an alias table is created. The alias table links the node names in the geometry to the node names from the modal data. This way the software can animate nodes on the geometry with the appropriate data (despite the geometry name and the data name not matching).  

 

In the Navigator worksheet of Simcenter Testlab, open the alias mapping table by right clicking on the project name in the project tree and selecting "Add/Edit Alias Mapping".

 

alias1.pngFigure 4: Right click on the project name and the click “Add/Edit Alias Mapping”.

The alias data and the original data must both be selected and mapped.

 

First, from the upper left, choose the "Active Project Geometry" as the alias data. The test measurement data will be mapped onto the selected geometry nodes.

 

aliasMap1.pngFigure 5: The alias mapping window.

Select the directions that need to be alias mapped. In this case, only the X, Y, and Z directions are of interest. Click “Replace”. This will import all of the geometry nodes and selected directions.

 

6.pngFigure 6: Chose the directions and import the geometry data.

Next, import the source measurement data that the geometry is to be mapped to. Using the selections in the upper right of the menu, this can either be from the active project or from the input basket. In this case, all the runs from a section in the active project are imported.

 

activeprojectdata.pngFigure 7: Select the original data and click “Replace” to import it.

Now the mapping must be completed. In this case, only the +X and +Y directions must be mapped (because data was only taken in the +X and +Y directions).

 

So, in the “Quick find” filter, search for +X in both the alias data and the original data.

8.pngFigure 8: Easily parse through data using the quick find feature. Any character can be searched on.

Knowing that “golfclub1:+x” in the geometry is equivalent to “club1:0+X” in the test data, these two nodes can be matched. Enter the nodes into the alias table by selecting the node from the list and then clicking the “Add” button. Repeat this for both the alias data and the original source data.

 

geom_and_test_map.pngFigure 9: Mapping the nodes to one another and populating the alias table.

Repeat this process until all necessary nodes are mapped. 

 

all_mapped.pngFigure 10: Map all nodes between the geometry and the test data.

NOTE: It is possible to copy and paste the alias table to / from excel. This would allows saving and restoring different configurations.To de-activate the alias table, highlight all the filled cells, right click, and choose "Clear".

 

 When the status is green and "Everything OK" message appears, press the "OK" button to continue.

 

Once all the nodes are mapped, it is possible to continue with the operational deflection shape or modal analysis and successfully animate shapes.

 

model.gifFigure 11: Animate mode shapes on the geometry.

NOTE: ALWAYS create the alias table before doing any modal analysis processing. The alias table will not override existing processing, it will only work for new processing.

 

The alias table makes linking the data names to the geometry names easier than ever!

 

Questions? Email jacklyn.kinsler@siemens.com or contact Siemens PLM GTAC support.

 

Modal Analysis and Operational Deflection Shapes links:

Comments
Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

For customers on maintenance, they can view a video on this feature on the GTAC site under Documentation for LMS Test.Lab.  There are several How To Videos.

 

https://support.industrysoftware.automation.siemens.com/docs/lms/test.lab/

2017-10-10 10_55_33-LMS Test.Lab_ Documentation_ GTAC_ Siemens PLM Software.jpg

 

 

 

Creator
Creator

Hi Friends!

 

I have a question.

The option "Alias Mapping" is available with the 17A Test.Lab version, but when I use the 16A version how is the procediment?.

 

Thanks in advance.

Alvaro

Siemens Legend Siemens Legend
Siemens Legend

Hi Alvaro,

Alias Mapping is not available in 16A, therefore, the data point id must match exactly on the Geometry->Nodes->Full name as shown here.

Picture1.jpgIf they're not matching, you could either modified the Geometry in Geometry workbook or modified your data point ID as shown here:

Picture2.jpgHong

Contributors