Cancel
Showing results for 
Search instead for 
Did you mean: 

Butterworth filter "regular" and "zero phase"

Siemens Theorist Siemens Theorist
Siemens Theorist

The Butterworth filter is a commonly known filter often used in online filtering (during the measurement) and introduces a typically undesired phase shift (delay) into the filtered data.

 

The length of the delay increases with decreasing cut-off frequency and increasing order. With increasing frequency (that is the frequency content of the signal) and filter order the phase shift becomes non-linear. That means the delay is not the same for all frequencies.

 

The red signal below has been filtered with a regular Butterworth filter at 50 Hz and a filter order of 8. You can clearly see the phase shift compared to the original (black) signal.

 

bw_reg.png

 

This phase shift can be prevented only if the complete signal is known in advance, which is impossible during a measurement.

 

Offline, this restriction obviously does not apply, here we can prevent the phase shift by going forward and backward over the signal to eliminate the phase shift. This is done when the setting zero phase is selected. You can see from the blue signal below that the phase shift is gone.

 

bw_zero.png

 

We have kept the regular mode in the software, since this is how the Butterworth filter is designed. The meaningfulness of its usage is rather an academic discussion.

 

Butterworth Filter in Simcenter Tecware Process Builder

 

There are two different methods in the Simcenter Tecware ProcessBuilder for the Butterworth filter, as shown below.  Simcenter Tecware ProcessBuilder can be run with Simcenter Testlab tokens.

 

butterworth.png

 

 

Depending on the desired phase characteristics, one or the other method can be use.

 

More detailed information on the Butterworth, direct, and zero phase filters can be found here: IIR versus FIR Filtering

 

Simcenter Tecware Links: