Cancel
Showing results for 
Search instead for 
Did you mean: 

Compare Runs in Simcenter Testlab

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

(view in My Videos)

 

run_comp2.pngWant to compare data from different runs quickly in Simcenter Testlab (previously called LMS Test.Lab)?

 

Want to calculate the average, standard deviation, or envelope of these runs?

 

It is all possible using the Run Data Averaging and Comparison Organizer in Simcenter Testlab!

 

The Run Data Averaging and Comparison Organizer (hereby referred to as Compare Runs) add-in in Simcenter Testlab is an excellent way to average and compare runs both online in the Measure workbook and off-line in the Compare Runs workbook.

 

Getting Started

 

Begin by going to Tools / Add-ins…

 

1.pngFigure 1: Go to Tools/Add-ins…

Select “Run Data Averaging & Comparison Organizer”. If using Simcenter Testlab token licensing, this uses 16 tokens.

 

2.pngFigure 2: The “Add-ins” window.

The add-in includes both online and offline functionality.

 

In either case, five averaging functions are added.

 

3.pngFigure 3: Definitions of the five functions.

This article is composed of two sections. The first section will cover the online functionality of Compare Runs. The second section will cover the offline functionality of Compare Runs.

 

SECTION 1: ONLINE RUN COMPARISON

 

After activating the Compare Runs add-in five averaging functions are added to the Measure workbook of Simcenter Testlab Signature.

 

4.pngFigure 4: The Measure workbook before and after the Compare Runs add-in is activated.

Compare Runs will also add information into the Data Explorer. Any 2D function that can be averaged will appear under the Compare Runs folder.

 

5.pngFigure 5: Explore the Compare Runs folder in Data Explorer to see what functions you can compare across runs.

Online Run Comparison Example

 

For this example, three runs were acquired.

 

Each run consisted of a single tone.

  • Run 1 was a tone of 1000Hz.
  • Run 2 was a tone of 1500Hz.
  • Run 3 was a tone of 2000Hz.

Each run was acquired using a stationary acquisition consisting of 13 averages over 3 seconds.

 

1. To begin, drop data into the display from the Compare Runs folder. In this case, a stationary autopower acquisition was done. So, there is an “AutoPower Mic” selection available. Drag from the LEFT pane into the display.

 

6.pngFigure 6: Any 2D functions will be available under the Compare Runs folder.

 

2. Next, select which averaging functions to display in the Measure workbook. For this example, the average function is displayed. Users can display any combination of the Compare Runs functions by toggling on or off the function buttons on the upper right of the plot display area.

 

7.pngFigure 7: Five functions are available with the Compare Runs add-in.

 

3. Under the “More…” button, there are three online averaging display options. For this example, “All runs” is selected.

 

8.pngFigure 8: Select which runs to display under the “More…” button.

A. “No run display” will not display any of the runs as they populate. The averaging functions selected will

 

B. “Last run only” will display only the most recently acquired run in addition to the averaging functions selected.

 

C. “All runs” will display all acquired runs in addition to the averaging functions selected.

 

 

4. The result after Run 1 (a tone at 1000Hz) is shown below. Run 1 is displayed in red. The average of all runs is displayed in black. In this case, the two curves are the same, so they overlap completely.

 

9.pngFigure 9: The first run and average of all runs are displayed. After only one run these values are the same.

5. The result after Run 2 (a tone at 1500Hz) is shown below. Run 1 remains displayed in red because the online averaging run display mode is set to “All runs”. As each run is acquired, the run will populate and remain as the additional runs are acquired. Run 2 is displayed in purple. The average of the two runs is displayed in black.

 

10.pngFigure 10: The display mode is set to “All runs”; the runs populate over one another and remain in the display.

6. The third and final run is then acquired (a tone at 2000 Hz). Run 3 is displayed in green. The original two runs remain in the display and the average function updates to include the third run.

 

11.pngFigure 11: The runs continue to populate in the display and the average function updates appropriately.

7. When finished acquiring data, go to the “Compare Runs” workbook. Here is where you will save the averaging functions across your runs. 1) Select which averaging functions you would like to be save by toggling the function buttons. 2) Press “Save…”

 

12.pngFigure 12: The Compare Runs workbook.

8. Users can either save just the selected functions or save all the functions. Name the folder then click OK to save.

 

13.pngFigure 13: Save the functions.

9. The functions will be saved to the folder in the Navigator workbook. In this case, just the average function was saved. Browse to the data block and display it.

 

14.pngFigure 14: Just the average function was saved.

10. If instead save “All functions” was selected, the function tree in the Navigator would look like below.

 

15.pngFigure 15: All functions are saved.

Online run comparison is a great tool to instantly check your run data average!

 

SECTION 2: OFFLINE RUN COMPARISON

 

It is possible to compare runs offline. These runs can come from any project or section.

 

In the offline mode, analysis begins in the Compare Runs tab.

 

16.pngFigure 16: Compare Runs tab.

The Compare Runs workbook has four main panes. 

 

17.pngFigure 17: Compare Runs workbook.

  1. Data Source Selection: import run data from the input basket or the active project.
  2. Run Selection: choose which runs to display and which runs to include in the averaging functions.
  3. Function Selection: a matrix of each Point ID and calculated function. From this matrix, choose what will be displayed the display pane.
  4. Display area: data plotted in this area is selected from the function and point matrix (area 3).

Data Source Selection

 

It is possible to import runs via the input basket or from the active project. Use the radio buttons to determine what the data source is.

 

18.pngFigure 18: Select to import from the Input Basket or Active project.

Once the data is imported, the Run Selection and Function Selection areas will populate.

 

19.pngFigure 19: The Run Selection and Function Selection areas are populated once the data is imported.

Run Selection

 

In the Run Selection area, there are two columns of checkboxes on the far right (see Figure 20).

  • The display column determines whether or not the run data is displayed in the display area on the right side of the screen (area 4).
  • The averaging column determines whether or not the run data is included in the averaging functions that are calculated.

It is important to note that a function may be included in the average even if it is not displayed. It is wise to inspect which of these boxes are checked before saving your averaged run data.

 

 20.pngFigure 20: The Display and Averaging columns determine which runs are displayed and which runs are used to calculate the averaging functions.

Function Selection

 

There are three different ways to display the functions: Point by Point, Function by Function, or User Defined Layout. To choose a display type, click either P,F, OR U in the lower right corner of the Function Selection area.

 

21.pngFigure 21: P: Point by Point. F: Function by Function. U: User Defined Layout.

  • Point by Point
    • Allows the user to display multiple functions calculated from the same Point ID.
    • 22.pngFigure 22: Multiple functions are displaying of the same Point ID.
  • Function by Function
    • Allows the user to display one function across multiple Point IDs.
    • 23.pngFigure 23: Multiple Point IDs are displaying for the same function.
  • User Defined Layout
    • The user defined layout allows the user to choose a custom mix of Point IDs and functions from the available options.
    • 24.pngFigure 24: A user-defined mix is selected.

NOTE:

 

In the user defined layout mode, there is one extra step to be aware of.

 

If a multi-plot display is opened, the number of plots in the display will correspond to the number of buttons that become sensitive to the left of the P, F, and U.

 

25.pngFigure 26: The user defined mode. Here the third graph is selected. The dotted line around the third plot indicates it is the active plot.

To select which functions to display, toggle the boxes in the upper right corner of the Function Selection area. The functions are defined at the top of the article in Figure 3.

 

27.pngFigure 27: The averaging functions are in the top right corner.

To control how many points/ functions are displayed, click on “Options…” in the Function Selection area.

 

Adjust the numbers for “Functions per display” and “Points per display”.

 

28.pngFigure 28: The Options window in Compare Runs.

Saving Average Run Data

 

Finally, save your data. Choose where to save your data, which functions to save, and what to call your new folder. 

 

29.pngFigure 29: The Save window in Compare Runs.

Enjoy the power of the Compare Runs workbook!

 

Questions? Email jacklyn.kinsler@siemens.com, contact Siemens PLM GTAC support, or post a reply!

 

Simcenter Testlab Acquisition Tips

Simcenter Testlab Processing Tips

Comments
Dreamer
Dreamer

Can I use the Compare Runs Add-In to average waterfall data as well?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Yes We Can … Here are the steps to do it

 

  • Use the ‘Data Source Selection’ on the Compare Runs Tab to your select waterfall data

A kb #25 p1.png

 

  • Next select which data will be included in the averaged together using the checks boxes in the “Averaging” column in Run Selection box

A kb #25 p2.png

 

 

 

  • Then using the upper left-hand corner of Function Selection box click on the all the functions you would like to calculate [ Average, Envelope Max and Envelope Min are all options]

A kb #25 p3.png

 

 

  • Then click on the ‘Options…’ button in the lower left corner of the Compare Runs tab

A kb #25 p4.png

 

  • To average waterfall data the option ‘Result X-axis values’ and ‘Result X-axis range’ need to be set to ‘From First run’ and ‘Intersection’ respectively.
  • Next press the ‘Close’ button on the Options box

 

A kb #25 p5.png

A kb #25 p6.png

 

A kb #25 p7.png

 

 

  • Now press the ‘Save’ button located bottom of the Compare Runs tab

A kb #25 p8.png

 

 

  • Then check the “Average waterfall data” box and press the ‘OK” button.
  • Then a progress bar will appear while the data is being processed

A kb #25 p9.png

 

A kb #25 p10.png

 

 

 

  • The average waterfall data will be saved in the active section in a folder named CompareRuns

A kb #25 p11.png

 

 

 

  • Know you can just drag and drop your averaged waterfall into a colormap display

A kb #25 p12.png