Cancel
Showing results for 
Search instead for 
Did you mean: 

History of Acoustics

Siemens Phenom Siemens Phenom
Siemens Phenom

History of Acoustics

 

1874 - Ernest Werner Siemens patents dynamic or moving coil microphone.

 

werner_siemens.jpgErnest Werner Siemens (1816-1892), founder of Siemens Corporation

The dynamic microphone did not become widely used at the time. Eventually, as technology improved, the dynamic microphone became the basis for most microphones used today. 

 

1877 – “Theory of Sound” textbook by Lord Rayleigh, the 1904 winner of the Nobel Prize in Physics, is published in the United Kingdom.

 

Rayleigh.jpgJohn William Strutt, 3rd Baron Rayleigh, 1842-1919

Lord Rayleigh discovered “Rayleigh Waves”, the sound waves that travel on a solid surface.  The acoustic impedence unit quantity “rayl” is named after him.

 

1877 – Third edition of “On the Sensations of Tone as a Physiological Basis for the Theory of Music” by Herman von Helmholtz (a friend of Ernest Werner Siemens) is published.

 

helmholtz.jpg1890 Helmholtz Resonator, Source: Physics Dept, Case Western Reserve University, Image credit Wikipedia

The book describes Helmholtz resonators, which are used to amplify specific frequencies based on a volume of trapped air (like blowing over an empty coke bottle).  Helmholtz used his resonators to isolate single tones of musical instruments.

 

1883 – The Indonesian island of Krakatoa experiences a volcanic eruption emitting what is considered to be the loudest sound ever heard in the modern world.  It is heard up to 3000 miles (4800 km) away from the eruption. 

 

kratatoa.jpgLithograph of 1883 volcanic eruption in Indonesian island of Krakatoa

Over 36,000 people are killed in the resulting tsunami, shock waves are recorded for days afterward, and the world climate was altered for years.

 

1924 – After approval from the “International Advisory Committee on Long Distance Telephony”, the Bell system renames the Transmission Unit (TU) into the decibel (dB). The decibel was named after the Bel, in honor of the telecommunications pioneer Alexander Graham Bell. 

 

dB_scale.pngDecibel (dB) scale for sound level

While the decibel unit was originally used to measure the loss in power in telephone cables, it later became widely used in acoustics to describe the level of a sound.

 

1930 – The “International Electrotechnical Commission” replaces “cycle per second” with “Hertz” as the SI unit of measure for repeated events per second, or frequency, in honor of Heinrich Hertz.  

 

hertz.jpgHeinrich Hertz, 1857-1864

Gustav Ludwig Hertz, the nephew of Heinrich, later became the research laboratory director at Siemens.

 

1930 - The Perrin Acoustic Array appears on the cover of Popular Mechanics.  The array, developed by French Nobel prize winner Jean-Baptiste Perrin, is billed as an "Airplane Finder Which Locates Ships in Flight, and Registers Their Altitude, Speed and Distance from the Apparatus".

 

perrin_acoustic_array.jpgPerrin acoustic array on cover of Popular Mechanics

The array is the forerunner of today's modern acoustic arrays

 

1933 – Fletcher-Munson Curves of equal loudness published in the “Acoustical Society of America” journal. The blue lines, represent the dB level required to have a tone sound equally loud to a listener at any given frequency.

equal_loudness.pngCurves of equal loudness - dB vs frequency. Blue lines represent equivalently loud levels

The curves of equal loudness have gone thru several updates.  In 1956, Robinson & Dadson updated them using a frontal speaker in an anechoic chamber.  In 2003, they were updated again as part of ISO  226:2003.

 

1936 – American National Standards Institute (ANSI) adopts the A-weighting curve based on Fletcher-Munson research in standards for sound level meters.

 

a_weight.pngA-weighting Curve - dB of attenuation vs frequency

The A-Weighting curve is used to introduce the effects of human hearing into microphone recordings.

 

1936 – Stanley Smith Stevens, professor at Harvard University, proposes unit for perceived loudness called Sones.

 

stanley_smith.pngStanley Smith Stevens (1906-1973) from the book “Stanley Smith Stevens” by George A. Miller, National Academies Press

The word Sone was derived from the Latin word sonus, which means sound.

 

1942 - Leo Beranek, working at Harvard, develops the first anechoic chamber.  An anechoic chamber is used to simulate an acoustic free field.  It this case, it was developed for testing loudspeakers for the US Army.

 

anechoic.jpgAnechoic chamber has fiberglass wedges to absorb sound so it is not reflected. Anechoic means "no echo".

Beranek also developed the metric Articulation Index (AI),which was used to understand how well speech can be understood over background sound.  AI was used in evaluating different models of headsets used in aircraft to make sure instructions from the ground could be understood.

 

1961 - The Bark scale, used to describe the logarithmic frequency groupings of human hearing, is proposed by Professor Karl Eberhard Zwicker of the Institute for Electro-Acoustics of TU Munich.

 

Critical_Bands.pngIn the bark scale, the critical bands of human hearing increase in width with frequency.

The Bark scale was named after Heinrich Barkhausen.  Zwicker also developed the DIN 45631 loudness standard.

 

1961 – Stanley Smith Stevens publishes “Procedure for Calculating Loudness: Mark VI”.

 

1963 – Only an acoustician! J.C.R Licklider, a psycho-acoustician and department of defense researcher, invents the internet (it was not Al Gore!)…OK, not quite...read on....

 

licklider.jpgJ.C.R Licklider, 1915-1990, acoustician and “Inventor of the Internet”

In 1963, Licklider secures funding to start building the “Intergalactic Computer Network” or ARPANet for defense department, the fore-runner of the internet.

 

1972 – Acoustical Society of America publishes “Perceived level of noise by Mark VII and decibels” by Stanley Smith Stevens.

 

home_depot.pngWant to experience sones? Head to Home Depot for the bathroom fan display

Stevens was the founder of Harvard's Psycho-Acoustic Laboratory.

 

1975 - ISO532 standard established for calculation of Loudness.

 

iso.pngISO Standards Organization logo

ISO532B outlines two methods of calculating loudness: a narrowband spectral approach and a 1/3 octave approach.  It also incorporates Zwicker masking.

 

1981 - ANSI incorporates B-weighting as well as the A-weighting curve.

BCDweighting.pngA, B, C, and D Weighting Curves

B-weighting is a flatter curve than A-weighting.  This mimics how the response of the human ear flattens with increased sound levels.

 

1981 - The ECMA-74 Standard for "Measurement of Airborne Noise emitted by Information Technology and Telecommunications Equipment" is published.

 

ttnr.pngTone-to-Noise Ratio

It includes standards for calculating Tone-to-Noise Ratio and Prominence Ratio.

 

1990 - Psycho-Acoustics: Facts and Models authored by Eberhard Zwicker and Hugo Fastl published by Springer.

 

psycho_acoustics.png3rd edition of Psycho-Acoustics by Hugo Fastl and Eberhard Zwicker

Psycho-acoustic content includes critical bands, masking, loudness, roughness, fluctuation, and more...

 

1994 – Actors Jeff Daniels and Jim Carrey introduce the “Most annoying sound in the world” in the movie Dumb and Dumber.

 

 

2000 - Directive 2000/14/EC (Outdoor Noise Directive - OND) is adopted by the European Parliament and the Council on July 3, 2000. The directive harmonizes the laws of the Member States on 57 types of outdoor equipment referring to noise emission standards.

 

equip.pngLayout of a sound power noise certification test for outdoor equipment

The world becomes a much quieter place as equipment manufacturers strive to meet the new noise regulations!

 

2008 - Fourteen year old Kyle Krichbaum correctly identifies 5 vacuum cleaners “by sound alone” on British TV show "Wanna Bet?", hosted by Ant and Dec...

 

 

 

Also need to analyze vacuum cleaner noise?  Try using Simcenter Testlab Sound Diagnosis.

 

Related Links: