Cancel
Showing results for 
Search instead for 
Did you mean: 

Import CAD Geometry into Test.Lab Geometry

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

(view in My Videos)

 

 

jet.png In LMS Test.Lab Geometry, it is possible to import a CAD file to the geometry instead of creating a geometry from scratch. Most CAD packages are able to export CAD geometry which the user can save locally.

 

File formats that are importable include:

  • Stereolithography files
  • Universal files
  • Nastran files
  • Virtual.Lab files (.VL2TL)

To import a CAD geometry into Test.Lab, open the Geometry workbook.

Go to Tools -> Add-ins and turn on “Geometry”.

 

Figure 1: The Geometry add-in uses 16 tokens.Figure 1: The Geometry add-in uses 16 tokens.

Browse to the geometry file in the file tree on the left of the screen.

 

Figure 2: Expand the geometry file directory to get to the component level.Figure 2: Expand the geometry file directory to get to the component level.

Click on the component(s) to import. Then select “Import Geometry”. This will overwrite any existing geometry in the project.

 

Figure 3: Import the geometry.Figure 3: Import the geometry.

The CAD geometry file will import.  The geometry that is imported can be used like any other geometry, from channel setup to animating mode shapes, etc.

 

Figure 4: Top: The .stl file is imported. Bottom: The .stl file can be used in channel setup to map nodes to channels.Figure 4: Top: The .stl file is imported. Bottom: The .stl file can be used in channel setup to map nodes to channels.

Often, the imported CAD geometry file contains many more nodes than locations that will actually be physically measured. If a node does not have associated measured data, it does not automatically animate. 

 

For example, the .stl file of the F16 aircraft that was imported in the example above has 1172 nodes. It is rare that 1172 measurement points would be taken so that every node in the geometry can be animated.

 

It can be confusing to only see the measured nodes moving and not the other nodes in the geometry – therefore animation extensions like “Automatic Topological” and “Automatic Geometrical” can be used. These extensions slave nodes together in the geometry so that more nodes animate than just the ones that have measured data associated with them.

 

Automatic Topological will look for nodes that are connected to other nodes. A connected node means that a line was drawn between the nodes in the Geometry workbook. The software algorithm animates any nodes that are connected to nodes with measured data associated with them.   

 

Automatic Geometrical will look at nodes that are near one another in space. The software algorithm then slaves the nodes together and animates the nodes.

To use these animation extensions, right click in a geometry window, go to “Animation Settings” and select either “Automatic Geometrical” or “Automatic Topological”.

 

Figure 5: Turn on visualization expansions.Figure 5: Turn on visualization expansions.

Look at the video below to see the difference between no modal expansion, Automatic Geometrical, and Automatic Topological. 

 

(view in My Videos)

 

Expanding the animation can be a great tool for reporting to make mode shapes and operational deflection shapes look more realistic.

 

Questions? Contact us!

 

Related Links:

Comments
Siemens Legend Siemens Legend
Siemens Legend

Great article!  One comment:  If your stereolithography file is ASCII it should have an *.stl extension, if it is BINARY then it requires an *.stlb extension.  If you are not sure, try both!  Or open in a text editor, if it's a BINARY file it will be pretty obvious.  If it takes a really long time to open then you should create a coarser STL file.

Visionary
Visionary

Hi,

I want to know I measured with minimum number of Accelerometer (sensors) with minimum node i imported a FEM model which has STL File format it has many nodes how to interpolate the nodes with minimum node test model and FEM STL model 

 

Kindly share a Notes and documents related to geometry topology 

Contributors