Cancel
Showing results for 
Search instead for 
Did you mean: 

LMS Tecware: Open time files fast!

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

(view in My Videos)

 

Open time files fast with LMS Tecware!

Did you know LMS Tecware has a feature that allows you to open time data directly from Windows Explorer into TimeEdit just by double clicking on the data?

 

This is possible with many different data types:

  • LMS LDSF
  • MTS RPC
  • nCode DAC
  • IST RigSys
  • More…

How?

 

This is an option that is presented during the installation of LMS Tecware.  However, if this was missed during installation, not a problem!

 

You can execute “create_shortcuts.exe” from the installed Tecware directory:

 

                C:\Program Files (x86)\LMS\LMS Tecware 3.12\create_shortcuts.exe

 

It will allow you to add start menu entries:

 

Picture 1: CreateShortcuts.exe can recreate Desktop shortcuts for ProcessBuilder and Tecware DesktopPicture 1: CreateShortcuts.exe can recreate Desktop shortcuts for ProcessBuilder and Tecware Desktop

and re-create the file associations between TimeEdit and various time data files.

 

 

Picture2: Create associations for TimeEdit to various time filesPicture2: Create associations for TimeEdit to various time files

More Files

 

Have a file that is not in the CreateShortcuts menu, but still supported by LMS Tecware?

 

No problem!  Additional files can be added by just right clicking on the file and selecting “Open with…”.

 

The associated program needs to be:

 

                <Tecware-Install-Dir>\bin\LMS TimeEdit.exe

 

Note: in the list of available programs, this shows up as “LMS Tecware” only, not “TimeEdit”. If it’s not in the list, use “Browse” to select "LMS TimeEdit.exe".

 

Picture3: Open with dialog for creating association with TimeEdit.Picture3: Open with dialog for creating association with TimeEdit.

Opening Files Fast

 

Go to the directory with the time files.  They will have Blue icons indicating that they will open with TimeEdit by default.

 

Just double click on the time file of interest.

 

Picture 4: Blue icons indicate file can be doubleclicked on and opened directly.Picture 4: Blue icons indicate file can be doubleclicked on and opened directly.

 

The file will be directly opened in TimeEdit for viewing and editing.

 

More Durability Links:

More Tecware tips:

Contributors