cancel
Showing results for 
Search instead for 
Did you mean: 

My LMS Smart Scope Favorites!

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

 

 

 

LMS Smart Scope Favoritesicon.png

 

 

LMS Smart Scope is the Android Tablet Companion application for the LMS SCADAS XS.  It is used to setup, control and analyze time file recordings acquired on the built-in mini-SD Card on the SCADAS XS.

 

There are a lot of cool features in LMS Smart Scope, but here are my favorites!:

 

1. Colormaps 

 

In the FUNCTIONS tab, click on the blue 2D/3D button to toggle between colormap and spectral data.

 

colormaps.png

 

Easy to view colormaps or spectrums while the test is in progress, or when analyzing data later.

 

2. Triggers

 

Trying to capture a specific event? Setup a start and/or stop trigger based on rpm, time, or level. When editing a template, setup up the trigger in the MEASUREMENT tab.

 triggers.png

 

For example, setting a trigger level of 0.5 g on a vibration channel with: 

  • Pre-Trigger of 2 seconds
  • Duration of 3 seconds

Results in a 5 second recording with the transient event located at exactly 2 seconds!

 

triggers2.png

 

This is possible because the SCADAS XS maintains a constant buffer of data equal to the Pre-Trigger time.

 

3. Unattended Acquisition

 

By default, after each acquisition is finished, the user is prompted to view, analyze, or accept the data. This is a manual operation, and requires user interaction.

 

If no user interaction is desired, the ‘Number of Runs’ parameter can be set in the MEASUREMENT tab of the template setup.  The LMS Smart Scope tablet software will automatically re-arm and take data for the specified number of runs.

 NumberOfRuns.png

 

This can be used in conjunction with start and stop triggers.  For example, data acquisition could be setup to acquire only when the rpm of an engine exceeds 1000 rpm.  This can even be taken one step further: no tablet!

 

Let’s say a new rollercoaster needs to be tested.  No one is allowed to be on the coaster, because it is brand new, and does not have safety belts installed. Setup the test (with triggers if so desired), start the measurement, and exit the Smart Scope software (by clicking on the back arrow multiple times).

 CloseApp.png

 

When asked ‘Close the Application: Do you want to still continue recording?’ say ‘Yes’.  The SCADAS XS can go off on the rollercoaster, while the test engineer stays safely on the ground.

cartoon_coaster.png

 

Once the SCADAS XS returns to within Wi-Fi range (150 feet line of sight approximately), just restart LMS Smart Scope to see the measurement in progress and review the data!

 

4. Sound Replay with Filtering

 

When analyzing recordings in the Measurements worksheet, they can be replayed thru the LMS Binaural Headset (which also can be used to record). 

 

headset.png

 

Listening can be done in the field immediately after a recording is finished.  In the replay menu, located at the bottom of the screen, different types of filters can be applied while listening.

filter.png

 

Filters include notch, bandstop, lowpass, and highpass. This makes it easy to identify and isolate that ‘annoying’ frequency that everyone is complaining about.

 

5. TEDS

 

Many accelerometers and microphones have an electronic chip with transducer calibration, serial number, and model number embedded into it.  This Transducer Electronic Data Sheet (TEDs) can be read by LMS Smart Scope by pressing the ‘Read TEDS’ button in channel setup.  

 

ReadTEDS.png

 

Select the channels and press ‘Done’.  This is very helpful when you have attached all your accelerometers to your test object and forgot to write down serial numbers and calibration values.  No need for a flash light and magnifying glass when you can just read the numbers directly into Smart Scope!

 

Conclusion

 

Thanks for reading about my favorite LMS Smart Scope features. Next step is to import the recorded time files from the mini-SD card into LMS Test.Lab for Throughput Processing!

 

Below you will find a PDF file of the ‘LMS Smart Scope Getting Started Guide’.  

 

Note: Some of these features required Version 5 Smart Scope or higher.

 

Related Links:

Contributors