Simcenter Testlab: Cursor Tips and Tricks

Siemens Phenom Siemens Phenom
Siemens Phenom

(view in My Videos)
 

 

New to Simcenter Testlab (formerly called LMS Test.Lab)?  Here are some cursor tips and tricks to get you started!

 

Adding a Cursor Readout to a Display

 

To add a cursor to an existing display, right click in the display while holding down the Control key (Picture 1) and select “Add Single Cursor -> X”. Right clicking without the control key requires clicking on the white background area of the graph, which is not always easy to do if there is a lot of data in the plot.

 

CursorLegend.pngPicture 1: While holding down CTRL-key, right click in display and choose “Add Single Cursor -> X” to add display to cursor.

A cursor should appear in the display.  Click and drag on the cursor to move it from left to right.

 

To see both the X and Y cursor values, select a curve by clicking on it, and a flag will be shown at the intersection of the data and the cursor showing the Y value.  Small black squares appear on the data curve to indicate it is selected. Clicking on the curve again (after it was previously selected) will deselect it.

 

SingleCursor2.pngPicture 2: Click on data to see cursor readout at intersection of data and cursor

Another method to show cursor X and Y values is to add a cursor legend to the display.  Right click in the display (while holding down Control-Key) and choose “Cursor Legend -> Auto” to add a cursor legend to the display (Picture 3).

 

CursorLegend.pngPicture 3: Right click in display and choose “Cursor Legend -> Auto”.

A cursor legend is added to the display. Values for all curves will be shown in the legend.  The legend can be moved by clicking and dragging on the top line of the legend.

 

Values can be exported to Excel by right clicking on the legend and choosing “Copy Values”.  The values can then be pasted into Excel.

 

Cursor Properties

 

Right click on the cursor and select “Properties” to change (Picture 4):

 

  • Cursor linestyle and color
  • Number of decimals used in cursor readout
  • Tooltip style
  • Add a label to the cursor

CursorProperties.pngPicture 4: Right click on cursor and select “Properties”

Moving the Cursor

 

Aside from clicking and dragging the cursor, it can be moved in several different ways.

 

For example, double click on the cursor and type in the desired position of the cursor.  It will move to this position (Picture 5).

 

CursorDoubleClick.pngPicture 5: Double click directly on cursor to type in desired cursor position manually.

One can also use the right and left arrow keys on the keyboard to move the cursor.

 

CursorArrowKeys.pngPicture 6: Right and left arrow keys control last selected cursor

If there is more than one Single X Cursor, the arrow keys move the cursor that was last selected.  The last selected cursor has extra arrow symbols at the top to denote this (Picture 6).

 

Moving to Maximum

 

The cursor can be moved to the maximum value of the data.

 

If there are multiple curves in the display, first select the curve to move to the maximum.  Do this by clicking on the curve once to select it.  Small black squares will appear on the curve to indicate that it is selected.

 

CursorGlobalMax.pngPicture 7: To move cursor to maximum of data, click on desired curve, then right click on cursor and choose “Move to Global Maximum”

Then right click on the cursor and select “Move to Global Maximum” as shown in Picture 7.  If the menu is insensitive, a curve in the display was probably not selected.

 

Snap to Data Values

 

When the cursor is being moved, it will float between data point and read interpolated data values between actual data points (Picture 8).

 

CursorInterpolate.pngPicture 8: Cursor reads interpolated value between actual data points.

If one desires that the cursor only read actual data values, right click on the cursor and choose “Snap to data points” as shown in Picture 9.

 

CursorSnap.pngPicture 9: Right click on cursor and choose “Snap to Data Values” to make cursor only display actual data points.

Because two different curves in a display may have different increments, it is necessary to select the curve for the Snap function.  This is done by clicking on the curve once. Small black squares appear on the curve to indicate it is selected.

 

Conclusion

 

Questions? Email peter.schaldenbrand@siemens.com or contact Siemens PLM GTAC support

 

Simcenter Testlab Display tips:

Comments
Experimenter
Experimenter

Hello,

There is some way to configure Cursor Decimals to 1 by default?  As I use 1 decimal, every time that I add cursor I need to set decimals manually from 2 to 1.

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes this is possible,

 

  •   right click in the display and select Options.  In the Options dialog on the Cursors tab, set the cursor Options to your preferences.  This will effect every future cursor.
  • use the Picture pulldown in the top right corner to Save a Layout.  If you choose a new name you can use the Create a Picture... button to select this layout.  If you overwrite the display or picture  layout (FrontBack assuming you using a FrontBack picture) then this will be your new default.  If you are saving a new default Layout I'd suggest removing any existing curves otherwise they will become reference curves in each picture.  You can also move the Legend and Cursor Legend above the display area and make any changes you wish at the  same time.
  • 2019-02-11 13_16_36-Inbox - kevin.grenier@siemens.com - Outlook.jpg2019-02-11 13_17_05-Inbox - kevin.grenier@siemens.com - Outlook.jpg
  • 2019-02-11 13_21_10-Save as Layout.jpg

 

Experimenter
Experimenter

Thanks Kevin! Smiley Happy