Showing results for 
Search instead for 
Do you mean 
Reply

Rectangular to round duct transition.

Is there any way to create a rectangular to round duct transition in 180 degree segments and bend lines so this can be fabricated in sheet metal? And if there is not when will this happen?

2 REPLIES

Hi Dave,...did your last transition topic cover this off?...

Hi Dave,...did your last transition topic cover this off?

[ie: ordered mode "lofted flange" using 180 degree sketch profiles, positioned accordingly]

Sean Cresswell
Design Manager Streetscape Limited
Solid Edge ST9 [MP7] Classic [x2 seats]
Windows 10

Re: Hi Dave,...did your last transition topic cover this off?...

Hi Sean,
Thanks for the followup. ordered seems to be the way to go with this particular transition in SE. I lean towards an aftermarket program though that allows me to set up my printer and use standard sheet sizes which it creates a layout and cut template from. Or at the least gives me all the flat co-ordinate points for layout from X-Y zero. Sheet lightning is the one and it is fine for thinner gages. Past say 11gage and I would go with Plate and Sheet as it gives layouts for inner center and outer of flange. SE is not quite there for what i want to do compared to these two programs.