Cancel
Showing results for 
Search instead for 
Did you mean: 

How stop new windows opening when dxf file is opened

Creator
Creator

I have a problem when opening dxf files a new solid edge window opens everytime. E.g.. 3 dxf files open, 3 separate solid edge windows. How do I change this to stop it from happening?

13 REPLIES 13

Hi there,   Are you getting a new window, or a new instan...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

Are you getting a new window, or a new instance per file?....what is it you want it to do??
As far as I know, it has always opened a new window per file. I had a quick glance through the import options and the registry, but couldn't spot anything that would control it to do anything differently.

 

This is how it reacts for me.... http://screencast.com/t/ZS5AT6Hr 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Solution Center article 002-7002869 addresses this, cut a...

Siemens Phenom Siemens Phenom
Siemens Phenom

Solution Center article 002-7002869 addresses this, cut and pasted below for your reference:


• Symptom
• ---------------
By default .DXF files are not associated to the Solid Edge ST3 application in
Windows 7. Using "Set your default programs" in Win 7 to associate .DXF files
with Edge.exe will result in launching multiple instances of Solid Edge ST3
instead of opening the .DXF files into a single, already running instance of
Solid Edge ST3.
• Hardware/Software Configuration
• Solid Edge ST3
Windows 7
• Solution
• To force Windows 7 to open .DXF files from Windows Explorer into a single
instance of Solid Edge ST3, add the following registry keys:

 

Windows Registry Editor Version 5.00

[HKEY_CURRENT_USER\Software\Classes\.dxf]
@="SolidEdge.DraftDocument"

[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.dxf]

[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.dxf\OpenWithList]
"a"="Edge.exe"
"MRUList"="a"

[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.dxf\OpenWithProgids]
"SolidEdge.DraftDocument"=hex(0):

 

 

I cannot upload a registry file to this site to allow you to quickly double-click to make the above changes but you can download a copy from this GitHub site

 

07/11/14 - edited to update URL linke

Re: Solution Center article 002-7002869 addresses this, cut a...

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

lines and instructions are missing from this solution:

1- what type of registry value do we have to create (string, binary, DWORD,...)?

2- value vs name not clearly indicated

3- what should I create in the 2nd branch mentioned for dxf and dwg (if anything)?

[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.xxx]

 

Here is what I tried:

test extension dxf.jpg

Re: Solution Center article 002-7002869 addresses this, cut a...

Siemens Phenom Siemens Phenom
Siemens Phenom

Simply follow the provided link in the solution to the githib site and *save* the provided registry fie from the link. Then double-click the downloaded registry file to implement the solution, Using the provided registry file will provide you with all the answers to your questions,

Re: Solution Center article 002-7002869 addresses this, cut a...

Valued Contributor
Valued Contributor

I get the following error when clicking on your link.

 

ERROR 404

There isn't a GitHub Page here.

Re: Solution Center article 002-7002869 addresses this, cut a...

Siemens Phenom Siemens Phenom
Siemens Phenom

Sorry, looks like GitHub changed some addresses.  Link has now been updated in the original post.

Re: Solution Center article 002-7002869 addresses this, cut a...

Valued Contributor
Valued Contributor

The link now works.  Thanks

 

Excuse me for being a novice when it comes to creating a new entry into the registry, but how do I get the info into the registry?  I tried saving the info out as a .reg file and importing it, but that gave me an error.  The info on the link makes it sound like this is already a program or a script.

 

I saved the info below as open_dxf_in_solid_edge.reg

 

[HKEY_CURRENT_USER\Software\Classes\.dxf]
@="SolidEdge.DraftDocument"

[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.dxf]

[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.dxf\OpenWithList]
"a"="Edge.exe"
"MRUList"="a"

[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.dxf\OpenWithProgids]
"SolidEdge.DraftDocument"=hex(0):

 

Re: Solution Center article 002-7002869 addresses this, cut a...

Siemens Phenom Siemens Phenom
Siemens Phenom

Mike,

 

You didn't copy and paste the *entire* registry file from the provided link ;-)

 

Try this and note the very first line, which is what is missing from your version:

 

Windows Registry Editor Version 5.00

[HKEY_CURRENT_USER\Software\Classes\.dxf]
@="SolidEdge.DraftDocument"

[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.dxf]

[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.dxf\OpenWithList]
"a"="Edge.exe"
"MRUList"="a"

[HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\FileExts\.dxf\OpenWithProgids]
"SolidEdge.DraftDocument"=hex(0):

Re: Solution Center article 002-7002869 addresses this, cut a...

Valued Contributor
Valued Contributor

Would it be possible to do this for DWG extensions as well?  Would the .reg file just need to be edited to swap out the DXF for DWG?

 

Mike