Creating an "outside dimensioned" L-Profile with the Flange feature

Phenom
Phenom

Hi all,

 

We sometime come across following type of flange:

E.g. L-profile; inside bend angle 135°, both flanges with outside dimensions need to be e.g. 100mm to the virtual intersection point.

 

I can't find a way to do this in NX.

 

In an old software we used to use for 3D CAD (Radan) we would do it like this:

2016-10-13_05.gifCreating a Flange (obtuse) in Radan 12016-10-13_06.gifCreating a Flange (obtuse) in Radan 22016-10-13_07.gifCreating a Flange (obtuse) in Radan2016-10-13_08.gifCreating a Flange (obtuse) in Radan; endresultI'm just pointing this out because I believe the Flange feature needs some "refreshing"

 

Any thoughts on this?

Huysmans Metalen n.v.
2x NX 12.0.2.9 Mach Designer
on Win10 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend