Cancel
Showing results for 
Search instead for 
Did you mean: 

Who Me Too'd this topic

Shortcuts in Plant Simulation 12

Creator
Creator

Hello,

 

I am opening this Topic because I prefer keyboard over mouse. This is why I like using shortcuts but since V12 I have a lot of troubles using shortcuts and keyboard controls.

 

Shortcuts:

Nothing is working like it did in V11. I hope this will be fixed soon. I tried already V12.1 but still the same behaviour since in V12

 

What is the problem?

Almost every shortcut does ONLY work if the class library is focused, which means it is working only once... This is not very helpfull while you want to switch between windows with Ctrl+Tab... Or if you want to use self defined shortcuts to arrange windows or if you want to close multiple windows (not all windows!!!) with Ctrl+F4.

 

Another point is the context menu handling in the class library. You can not open a context menu with the keyboard anymore! You need to use a mouse Smiley Sad

 

Please let me know if you are already working on this one. Thanks.

 

Who Me Too'd this topic