Cancel
Showing results for 
Search instead for 
Did you mean: 

Who Me Too'd this topic

ER 7851802 - Bend lines with angle information

Legend
Legend

Good day everyone, with this topic I would like to see if we are the only one with this reqeust. Also if possible I would like to gather as much support from the community as I can get ofcource. This case is 1 out of 2 of our biggest wishes in our wishlist in Solid Edge.

 1 Gpi logo.png

 

Company: GPI

Website: www.gpi.nl

 

System:

Windows 10 Professional

Solid EdgeST8 – MP12

 

Solid Edge seats:

GPI – Division Netherlands:  11 Seats.

GPI – Division Poland:  5 Seats.

 

Our product contains an 100% custom made dynamic environment in Solid Edge.

 

2 Gpi uitleg.PNG

Problem case

For this problem I took an project that was easy to compare. These two projects have the most resemblances with each other, to have the best case with improving lofted flange.

 

Solid Edge:

3 Solid edge tekening.png

 

 

Autocad:

4 Autocad tekening.png

 

Solid Edge: Lofted flange flatten with bend table.

5 Solid edge bend table.png

Autocad: Produced cone from an lisp that gave the bending line and angle.

6 Autocad bend uitslag.PNG

 

The lisp has been made approx 15years ago, and till today SE doesn't provide any information about bending lines within the lofted flange.

 

I have tested it in ST10, and because of that I now would like some opinions from the community.

Sander
The Netherlands
Who Me Too'd this topic