Cancel
Showing results for 
Search instead for 
Did you mean: 

Who Me Too'd this topic

ST10 issue with assemblies

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

We just upgraded to ST10 late last week. Some users are seeing a problem with assemblies where they single left click on a component in the pathfinder as you might do if you wished to look at related constrains for example. However, instead of just hilighting the component and showing the constraints and the two ribbons that pop up  (edit in place and move) it immediately inserts another instance into the assembly. Mine did it yesterday but not today so far but two others are complaining today.

I have a vague impression that I've heard of this here but I'm not certain and can't find anything related in searches. Does this ring any bells?

Edit: Since I just discovered that we have the Win10 Fall Creator's update is it probable that this is being caused by the resultant slow dialog generation?

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200
Who Me Too'd this topic