Cancel
Showing results for 
Search instead for 
Did you mean: 

Who Me Too'd this topic

Hiding the "Parallel Generate" option

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

While I realize this is NOT for everyone, and the default value should be to show it...

 

I, and some other users here, find "Parallel Generate" to be more of an annoyance than a help (we typically have small toolpaths that only take a few seconds to generate, _maybe_ a couple that take 30 or more seconds per part)

 

And it is way too easy to right-click -> and accidentally select "Parallel Generate" instead of "Generate".

As we are in Teamcenter, dealing with the dialogs to kill the parallel generate sometimes takes longer that a straight "Generate" would have taken.

 

I created an ER to allow us to hide the "Parallel Generate" option (ER 9068136) (I'm assuming as a customer default, but it could be a preference or whatever).

If you find this annoying too, feel free to file a "me too" ER with GTAC

Thanks for your time...Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Who Me Too'd this topic